Mouser Now Shipping TDK InvenSense SmartIndustrial Sensor Family for Variety of Industrial Applications
May 3, 2021 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now offering the SmartIndustrial™ sensor family from Invensense, a TDK Group company. These compact, high-precision, low-cost, accelerometers and motion-sensing microelectromechanical systems (MEMS) modules give engineers a range of sensing choices for industrial applications, including robotics, tilt sensing, platform stabilization, navigation, industrial automation, and much more.
The SmartIndustrial product family, available from Mouser Electronics, include the IIM-42351 and IIM-42352 sensors. The very-low-noise 3-axis accelerometers feature digital-output programmable ranges up to ±16g in a small 2.5 mm × 3 mm × 0.91 mm, 14-pin LGA package. The IIM-42351 accelerometer enables precise tilt-sensing of industrial and Internet of Things (IoT) devices such as robotic arms, AGVs, utility poles and cameras. The IIM-42352 accelerometer measures wide-range vibration frequencies up to 4 Khz, enabling predictive maintenance of rotating equipment like pumps, motors, and compressors, to help identify failures before they happen.
The IIM-42652 is the smallest, most cost-effective, and lowest-power 6-axis inertial measurement unit (IMU) within the SmartIndustrial product line. Featuring the same dimensions and 3-axis accelerometer performance as the IIM-42351 and IIM-42352, the IIM-42652 also includes a digital-output, 3-axis gyroscope that offers a programmable full-scale range of ±15.625°/second to ±2000°/second. The compact module supports an extended operating temperature range up to 105°C, enabling engineers to design it into a wide range of industrial IoT applications, including navigation and stabilization of industrial machinery and robots.
Coming soon from Mouser are the IIM-46230 and IIM-46234 6-axis MotionTracking® devices, offering easy, robust, and accurate inertial measurements for industrial applications. The devices include the proprietary TDK SensorFT™ (Fault Tolerance) feature, which delivers built-in redundancy and early warning capabilities.
The IIM-42351, IIM-42352, and IIM-42652 are supported by evaluation and development kits, also available from Mouser Electronics. Each device's evaluation kit offers a fully assembled and tested evaluation board that can be used as a stand-alone board or connected to the corresponding development kit. Each development kit features a hardware unit for evaluating the respective SmartIndustrial sensor as well as all necessary software.
To learn more about the SmartIndustrial sensors, visit https://www.mouser.com/new/tdk/tdk-smartindustrial-sensor-platforms/.
As a global authorized distributor, Mouser offers the world's widest selection of the newest semiconductors and electronic components — in stock and ready to ship. Mouser's customers can expect 100% certified, genuine products that are fully traceable from each of its manufacturer partners. To help speed customers' designs, Mouser's website hosts an extensive library of technical resources, including a Technical Resource Center, along with product data sheets, supplier-specific reference designs, application notes, technical design information, engineering tools and other helpful information.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an authorized semiconductor and electronic component distributor focused on New Product Introductions from its leading manufacturer partners. Serving the global electronic design engineer and buyer community, the global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 1,100 manufacturer brands. Mouser offers 27 support locations worldwide to provide best-in-class customer service in local language, currency and time zone. The distributor ships to over 630,000 customers in 223 countries/territories from its 1 million-square-foot, state-of-the-art distribution facilities in the Dallas, Texas, metro area. For more information, visit https://www.mouser.com.
About TDK InvenSense
InvenSense, Inc., a TDK Group company, is a world leading provider of MEMS sensor platforms. InvenSense's vision of Sensing Everything® targets the consumer electronics and industrial areas with integrated motion and sound solutions. InvenSense's solutions combine MEMS (micro electrical mechanical systems) sensors, such as accelerometers, gyroscopes, compasses, and microphones with proprietary algorithms and firmware that intelligently process, synthesize, and calibrate the output of sensors, maximizing performance and accuracy. InvenSense's motion tracking, audio and location platforms, and services can be found in mobile, wearables, smart home, industrial, automotive, and IoT products. In May of 2017, InvenSense became part of the MEMS Sensors Business Group within the newly formed Sensor Systems Business Company of TDK Corporation. InvenSense is headquartered in San Jose, California, and has offices worldwide.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com