Osram Osconiq S 3030 QD LEDs with High-Efficiency Quantum Dot Technology Now at Mouser Electronics
August 1, 2019 - Mouser Electronics, Inc., the authorized global distributor with the newest semiconductors and electronic components, is now stocking Osconiq® S 3030 QD LEDs from Osram Opto Semiconductors. Utilizing Quantum Dot (QD) tunable light conversion technology, these mid-power LEDs are designed for area lighting and downlight applications that benefit from high efficacy and excellent color rendering.
This product is Osram's first LED to feature QD technology, which delivers outstanding efficacy, even at high color rendering indexes (CRI). It enables Osram to begin to close the efficacy gap that exists between CRI 80 and CRI 90 LEDs today. Another unique feature of the Osconiq S 3030 QD is the QDs are encapsulated to protect them from moisture and other external influences that pose the greatest risk to the functionality of an LED.
Osram Osconiq S 3030 QD LEDs, available from Mouser Electronics, offer illumination color options of warm white or cool white (2,700 K to 4,000 K) with a minimum CRI of 90. The LEDs' innovative QD phosphor solution enables CRI 90 to achieve an outstanding efficacy value of 173 lm/W at 3000 K, a best-in-class value for 0.2 W high-performance LEDs. The devices can withstand up to 8 kV of electrostatic discharge (ESD) voltage according to ANSI/ESDA/JEDEC JS-001 (HBM, Class 3B).
The Osconiq S 3030 QD LEDs are housed in a compact 3 × 3 mm surface-mount package and offer a wide 120-degree beam angle at 50 percent luminous intensity. The LEDs feature luminous flux of 31 lm at 3000 K with a forward voltage of 2.75 V, forward current range of 10mA to 180mA, and an operating temperature range of minus 40 to 100 degrees Celsius.
To learn more about lighting trends and product information, visit Mouser's Lighting Applications site at www.mouser.com/applications/lighting.
To learn more about Osram Osconiq S 3030 QD LEDs, visit www.mouser.com/osram-osconiq-s-3030-qd-leds.
With its broad product line and unsurpassed customer service, Mouser strives to empower innovation among design engineers and buyers by delivering advanced technologies. Mouser stocks the world's widest selection of the latest semiconductors and electronic components for the newest design projects. Mouser Electronics' website is continually updated and offers advanced search methods to help customers quickly locate inventory. Mouser.com also houses data sheets, supplier-specific reference designs, application notes, technical design information, and engineering tools.
About Mouser
Mouser Electronics, a Berkshire Hathaway company, is an award-winning, authorized semiconductor and electronic component distributor focused on rapid New Product Introductions from its manufacturing partners for electronic design engineers and buyers. The global distributor's website, Mouser.com, is available in multiple languages and currencies and features more than 5 million products from over 750 manufacturers. Mouser offers 26 support locations around the world to provide best-in-class customer service and ships globally to over 600,000 customers in more than 220 countries/territories from its 750,000 sq. ft. state-of-the-art facility south of Dallas, Texas. For more information, visit www.mouser.com.
About OSRAM Opto Semiconductors
OSRAM, based in Munich, is a leading global high-tech company with a history dating back more than 110 years. Primarily focused on semiconductor-based technologies, OSRAM's products are used in highly diverse applications ranging from virtual reality to autonomous driving and from smartphones to networked, intelligent lighting solutions in buildings and cities. OSRAM utilizes the infinite possibilities of light to improve the quality of life for individuals and communities. OSRAM's innovations will enable people all over the world not only to see better, but also to communicate, travel, work, and live better.
Trademarks
Mouser and Mouser Electronics are registered trademarks of Mouser Electronics, Inc. All other products, logos, and company names mentioned herein may be trademarks of their respective owners.
Kevin Hess, Mouser Electronics
Senior Vice President of Marketing
(817) 804-3833
Kevin.Hess@mouser.com
Kelly DeGarmo, Mouser Electronics
Manager, Corporate Communications and Media Relations
(817) 804-7764
Kelly.DeGarmo@mouser.com